We have placed cookies on your computer to help make this website better. You can change your cookie settings at any time. Otherwise, we'll assume you're OK to continue.

TOTAL STATIONS FOR EVERYDAY JOBSITE USE - NOW WITH ENHANCED SOFTWARE

Hilti POS 180 and POS 150 Robotic Total Stations

Press Contact

Carla Biggs

(972) 403-5927

Email
TULSA, Okla. – March, 2014 - Hilti has enhanced the software functionality of their POS 180 and POS 150 Robotic Total Stations by focusing on an easy to use interface which provides users the ability to import CAD information directly into the POC 100 controller. This new software helps save time with new “fly out” menus within the plan screen in order to zoom, create, select and edit points, extract points from CAD elements, and create arcs from points—all using just a fingertip—no pen needed.

While the Hilti POS 180 and POS 150 Robotic Total Stations have always stored digital plans in memory, and had a compact controller in permanent wireless contact with the total station to provide direct access to functions, this enhanced software will help make everyday layout and measuring tasks easier than ever before.

With intuitive operation and automatic target acquisition, the Hilti POS 180 and POS 150 Total Stations are great for 3D layouts: outdoors on the ground or on facades, indoors on floors, ceilings and walls, and for checking positions on plans and measurements for drawing up building plans.

The POS 180 and 150 bring the whole jobsite to your fingertips by providing a reliable “Building Information Modeling (BIM) to the jobsite” and “jobsite to BIM” data flow. Thanks to automatic prism tracking and continuous measurement data capturing, the new controller puts the complete building plan in the palm of your hand.

This free upgrade to existing tools in the market will be available on April 1 and will be shipped with all new tools beginning on April 1 as well.

Backing the Hilti POS 180 and POS 150 Robotic Total Stations is Hilti’s Calibration Service to help ensure reliability and accuracy. Even with Hilti’s built-in protection features, precision instruments can be affected by everyday use and more. Through the Calibration Service, the total station will be calibrated and adjusted as needed, with the calibration confirmed in writing. The POS 180 and POS 150 Robotic Total Stations also are covered by Hilti’s Lifetime Service, a unique service agreement that includes two years of no-cost coverage*.

For more information about the Hilti POS 180 and POS 150 Robotic Total Stations, please contact Hilti Customer Service. From the United States, call Hilti, Inc., at 1-800-879-8000 or visit www.us.hilti.com; from Canada, call Hilti (Canada) Corporation at 1-800-363-4458 or visit www.hilti.ca. *Some limitations apply. Contact Hilti for details.

About Hilti, Inc.

Hilti is a world-leading manufacturer and supplier of quality, innovative and specialized tools and fastening systems for the professional user. With more than 1,500 highly trained Hilti account managers and engineers throughout North America and an additional 1,300 Hilti employees nationwide, Hilti expertise covers the areas of powder actuated fastening, drilling and demolition, diamond coring and cutting, measuring, firestopping, screw fastening, adhesive and mechanical anchoring, and strut and hanger systems.