Hilti
Hilti USA
(866) 445-8827
| EN | ES

Go

CP 680 family of cast-in firestop solutions


Hilti, Inc. has announced the addition of three new Cast-in Firestop devices. These new products compliment the existing Hilti Firestop product offering, particularly the line of CP 680 Cast-In Firestop Devices. The new solutions allow for a quick and easy method of firestopping several unique plumbing applications. The highly innovative, UL tested, plumbing solutions utilize devices that are set to the construction forms prior to pouring concrete.

Hilti CP 681 Tub Box Kit

The CP 681 Tub Box Kit allows easy placement for tub drain and overflow piping by providing a recessed area in the concrete slab. The sleeve, through which the tub drain piping is passed, is fully firestopped thus eliminating the need for additional materials such as caulks or sealants.
Read more about Hilti's CP681 Tub Box Kit

Hilti Firestop Aerator Solution


The unique Hilti Aerator Solution provides a recessed area from the underside of concrete decking for installation of single stack waste pipe system aerators. The system utilizes a CP 680 Cast-in Device and an innovative adapter that allows sufficient space for the aerator to be installed close to the deck, simplifying ceiling installation.
More details about Hilti's aerator adapter

Hilti Firestop Shower Drain Solution


The innovative Shower Solution, in addition to providing easy installation of piping through floors, also allows for increased pipe movement after placement.

Hilti CP 680 Cast-In Firestop Device

The original member of the Hilti cast-in family of UL tested firestop products, the CP 680 is an innovative, one-step firestopping solution for a variety of penetrating applications. Available in three sizes, it is ideal for many through penetrations such as metal and plastic pipes, electrical cables and cable bundles. Its uses include both poured concrete floors and concrete over metal decking.
Go to the CP 680 P/M product pages